Briowireless – Turning your IoT project into reality


Based on the Gemalto modules, Briowireless’ BitPipe family facilitates integration of wireless connectivity to your IoT solution. The BitPipe devices are a combination of the BitPipe IoT interface and Modem family and provides flexibility needed to adapt to your IoT solution quickly and accelerate your time to market. The BitPipe devices have two modes of […]

B+B SmartWorx : SMART CHOICES in Cellular Routers


Select the Router That’s Right for You. When choosing a cellular router you don’t want to invest in features that you don’t need. But you don’t want to limit your options either. That’s why the B+B SmartWorx family of intelligent cellular routers offers you such a wide range of interfaces, capabilities and smart choices. Whatever […]

Sierra Wireless – Deploy on the fastest LTE networks in the world


Sierra Wireless AirPrime® EM7455 LTE-Advanced module offers unprecedented LTE speeds, bandwidth, and network performance on the M.2 standards-based form factor. The EM7455 supports most 4G LTE bands in the market providing coverage for the Americas and EMEA on a single SKU (and all of APAC on the EM7430 SKU). With automatic fallback to 3G networks […]

MultiTech – Industry-Certified, Developer Friendly Embedded Cellular SoM


MultiTech’s MultiConnect® Dragonfly™ cellular System-on-Modules (SoM’s) are complete, ready-to-integrate modules that offer developers the functionality of a programmable computing platform with the convenience of an onboard cellular radio all in one compact design. From a software perspective, Dragonfly is compatible with the ARM® mbed™ programming platform allowing for rapid prototyping and development. With its integrated […]

MultiTech – Programmable Gateway for the Internet of Things


MultiTech’s new IoT platform includes programmable gateways, long-range RF modules, accessory cards, and a remotely hosted application marketplace with comprehensive device management. MultiConnect® Conduit™ is the industry’s most configurable, manageable, and scalable cellular communications gateway for industrial IoT applications. Network engineers can remotely configure and optimize their Conduit performance through DeviceHQ™, the world’s first IoT […]

MultiTech – New 4G-LTE SocketModem® Cell Embedded Modems, Certified and Approved for M2M/IoT Applications


MultiTech has expanded its portfolio of embedded cellular modems and announces the availability of its first 4G-LTE models for the SocketModem Cell family. Models supporting AT&T, Europe and Verizon Wireless are now available. SocketModem Cell embedded cellular modems are network ready-to-integrate and carrier approved as an end device. These communications devices use the same Universal […]

Digi – Security and Performance for Digital Signage and M2M Terminals with Digi International’s TransPort™ WR11 4G LTE Routers


The Digi TransPort™ WR11 gives network management professionals a secure, reliable, and low-cost 3G/4G LTE connection to retail terminals for digital signage, kiosk, vending and gaming applications. Digi TransPort™ WR11 comes with Digi’s enterprise software configuration by default, which means network administrators have the routing, security, VPN and stateful firewall tools they need to create […]

MultiTech – MTSMC-H5: Fully certified, carrier approved cellular connectivity for your M2M/IoT Application


The SocketModem® Cell embedded cellular modem is ideal for customers looking to add cellular communications to their device or solution. This carrier approved and end-device certified embedded cellular modem offers a universal socket footprint that assures a seamless migration to future technologies. This design approach spans across all major cellular technologies, and provides a long […]

Multitech – Multitech’s MultiConnect® rCell – More Than Just A Router!


The MultiConnect® rCell 100 Series of cellular routers are a part of MultiTech’s comprehensive portfolio of cellular connectivity products optimized for M2M (machine-to-machine) communications. With a powerful remote Device Management platform, active on all MultiConnect rCell 100 Series routers, truck rolls are a thing of the past! Optimizing efficiency and providing the most compelling return […]

Sierra Wireless – Sierra Wireless AirPrime® Embedded Modules HL Series


Compact, Flexible, and Future Proof 2G, 3G, and 4G Essential Modules. Sierra Wireless AirPrime® HL embedded modules offer everything device manufacturers need to meet essential connectivity requirements for machine-to-machine (M2M) applications such as healthcare, point of sale terminals, fleet management, tracking, and consumer electronics. Key differentiators include a common form factor, small size, low-power consumption, […]